Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Drawing sheet's resize commands for lines ?

Genius
Genius

Hello

Drawing sheet: Is there a simple resize command in NX for lines. (Same as MsPaint's "Resize": Percentage)

  • For example resize lines +50% (=enlarge 50%).

I have *NX 11 Wizard* converted drawing sheet .DXFs to .PRTs(=lines and arcs.) and now I want to scale the converted drawings differently.

  • I have previously used the same paper size and scale as original .DXFs.

For example:

  • Original DXF is A1 and 1:10.
  • I want to change the "wizarded" .PRT to A2 and 1:20.

 

Thanks

1 REPLY 1

Re: Drawing sheet's resize commands for lines ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @12131444 ,

 

Your query looks similar to this: Scale lot of curves in sketch

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!