Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing symbol Error!!!!!!

Hello All,

I just typed < 0,1% in spreadsheet. When I switch to drawing sheet tabular note, it shows error. Pictures are attached.

I have checked for text format in both spreadsheet and drawing table tabular note. Its all fine. Somehow Im getting this error. Not sure Why!!Man Indifferent

Thanks,

Devaraj1.JPG23.JPG

4 REPLIES 4

Re: Drawing symbol Error!!!!!!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Instead of <0,1%, try $<0,1%. The characters < and > are special in NX, they are used for text formatting much like HTML tags are used for webpages. The $ character escapes the special character and tells NX to treat it as a normal character and not as a tag.

Re: Drawing symbol Error!!!!!!

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Devraj_Mendon,

Type it as "$< 0,1 %"
< , > are used to define control characters to format text in NX. Adding "$" sign before "<" will work in such cases.

Re: Drawing symbol Error!!!!!!

Thank you guys, It works!!Man Happy

Devaraj



 

Re: Drawing symbol Error!!!!!!

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Devraj_Mendon,

 

Here's the relevant documentation on Using Control Characters to Generate Symbols.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration