Cancel
Showing results for 
Search instead for 
Did you mean: 

Dynamic Assembly Load Options on opening part

Builder
Builder

 

Dear Community

 

is there a way to "quick-load" a closed component from an assembly by applying a command "open from folder OR open as saved" to it without going to change the session behaviour on the assembly load option?

 

Many thanks for your hints

 

 

_____________________________
Are you familiar with my product?
click here
3 REPLIES

Re: Dynamic Assembly Load Options on opening part

Phenom
Phenom
Hi,


We can suggest different solutions ,  but before we need understand with an example the work flow of your work with Nx.


What do you mean for dynamic and in which case you need a switching of load options?




Inviato da Outlook per Android
Thank you...

Using NX 11 / RuleDesigner PDM

Re: Dynamic Assembly Load Options on opening part

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @mascaritas,

 

You have to make your changes using the Assembly Load Options, which as you know are applied to the session.  While you can open and close individual components, using the Assembly Navigator, you cannot apply unique (or individual) load options to "quick load" a component on-the-fly.

 

Regards, Ben

Re: Dynamic Assembly Load Options on opening part

Builder
Builder

Hi thanks for the hint

 

A nice approach would be that if a part cannot be loaded with the session load option, that the "as saved" option becomes temporarly available on the same dialog, without going to through all the menus.

 

Greetings

_____________________________
Are you familiar with my product?
click here