Cancel
Showing results for 
Search instead for 
Did you mean: 

ER: Add ability to specify relative paths in assembly load options

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Below find an ER of mine, if you find it useful, feel free to ask GTAC to be added to ER#7331909.

Short Description of desired enhancement: <Problem rather than a solution>

    It is not possible to use relative paths for search folders.

What activity in your process is the product not able to currently handle?

    I want to specify search folders relative to the location of the assembly part files.

What result are you trying to achieve? (Please provide as many details as possible.)

    I want to specify the folder to search for components relative to the folder of the assembly part file location.

Do you currently have a workaround?
    No.

Do you have a proposal for the solution you envision Siemens PLM providing for this capability?
    
What is the level of productivity gained from such an enhancement?

    HIGH, easier way to specify search folders in a structure folder structure.

Other information:

    We do have a structure folder structure to save NX part files separated by departments (shop floor, nc programming, design, etc.)

    Sample folder structure:
project
|
+-CAD
|
+-CAM
|
+-CNC

The CAM and CNC departments are using the CAD parts as components through the master-model concept, so the search folder should contain the relative path "..\CAD", but that doesn't work currently.
"As Saved" doesn't work, since I have standard parts that are version specific, so I need search folders.
Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
3 REPLIES

Re: ER: Add ability to specify relative paths in assembly load options

Legend
Legend
how do you request to be added to an existing ER?
Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: ER: Add ability to specify relative paths in assembly load options

Phenom
Phenom
It's been a while for me, but I would call GTAC and ask them to add me to that ER. It might not be their preferred method, but that is where I'd begin.
-Tim

Re: ER: Add ability to specify relative paths in assembly load options

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

@R_Newcomb,

 

Open a new IR with GTAC (QTAC or phone) and request that your IR is closed against existing ER# 7331909.

Regards, Ben