Cancel
Showing results for 
Search instead for 
Did you mean: 

ERROR OPENING PRT FILE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

 

One of my user is facing an issue regarding .prt file opening whenever he tries to open hes getting a meesage Capture.JPG

 

so what should we do in this case because when i tried to open in my pc its opening without any issue and another issue is he created some parts last month and when he is trying to open the same issue hes getting.

and also i tried this using cmd nx tools to inspect even that is not working either

 

Any suggestions!!

 

 

 

 

Thanks in advance

3 REPLIES

Re: ERROR OPENING PRT FILE

Siemens Creator Siemens Creator
Siemens Creator
Have you tried moving the file to another location (i.e c:\nx\) to se if the same problem occurs?
Does the user have the correct access rights to the specified folder/files?

Re: ERROR OPENING PRT FILE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
yes i tried all the posibilities but none works..


Thanks for the reply @LarsMEriksson

Re: ERROR OPENING PRT FILE

Siemens Phenom Siemens Phenom
Siemens Phenom

HI @karthik6,

 

I would follow the instructions and open an IR with your local GTAC office and upload the part file to see if it can be fixed.

 

Regards, Ben