Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

EasyFill Installation

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello Experts,

I'm trying to install EasyFillAdvanced for NX12, but can't get it to show in my Application Ribbon.

I followed the instructions here, but still, the ribbon doesn't show up.

 

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/MoldWizard-amp-NX10-problems/m-p/297...

 

In the end, I believe I should end up with something like this (see attached)Capture.PNG

Can anybody enlightened me on that one please?

Thanks!

Jack.

2 REPLIES 2

Re: EasyFill Installation

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @JacquesL,

 

Your expectation is correct - you should see a tab on your ribbon.

 

1) Make sure you have at least NX 12.0.1 mp4 or NX 12.0.2 installed.

2) Set environment variable MOLDWIZARD_DIR to your moldwizard directory

3) Install the Moldex3D exectuables, that come with EasyFill, as administrator

4) Restart your workstation

 

Screenshot - 12_6_2018 , 4_10_35 PM.png

 

Note the requirement in the EasyFill readme file:
* Please check whether "simulation pre/post application" has been installed.

 

Regards, Ben

Re: EasyFill Installation

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

@BenBroad That worked! I also had to replace and add the easyfill files in the moldwizard folder, instead of having a subfolder (i.e. ~\moldwizard\easyfill\...).

Cheers,

Jacques