Cancel
Showing results for 
Search instead for 
Did you mean: 

Edge curves from colored surfaces

PLM World Member Creator PLM World Member Creator
PLM World Member Creator

Hello,

 

This is imported parasolid data and it is a single solid.  I have manually colored the golden colored faces and would like to extract the edge curve where the two (gold/blue) colors meet.  I'm using NX9.0.3.4 on a ADV5XMACH licnese bundle.

 

The image is just a portion of my model and the golden area travels all over the part.  Picking each edge curve is/was a bit laborious and i'm looking to streamline this process.

 

Thanks in advance.

 

Jerry

2 REPLIES 2

Re: Edge curves from colored surfaces

Legend
Legend
I generally use extract geometry to copy the faces to another layer then pull the curves off of those newly extracted faces.

You can select by color with extract geometry.
Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: Edge curves from colored surfaces

PLM World Member Creator PLM World Member Creator
PLM World Member Creator

That works, Thanks!