Cancel
Showing results for 
Search instead for 
Did you mean: 

Edit Mechanical Routing Path

Experimenter
Experimenter

Is it possible to edit a mechanical routing path once it is created? I often have to design a lot of tube routings and since the design is immature, the routing path often changes. But in order to mate to the new part, it seems like I have to create an entirely point set and then create a new routing path through those points. Is that correct or is there an edit option that I'm not seeing?

 

Working in NX-11

2 REPLIES

Re: Edit Mechanical Routing Path

Siemens Legend Siemens Legend
Siemens Legend
Can you illustrate this in some way ?
To me, most everything is editable.
( Routing has it's pro's and con's.)

Regards,
Tomas

Re: Edit Mechanical Routing Path

Legend
Legend

As I think, you used Spline Path to create the tube path.
If you have problem to move define point by Dynamic handle, you must check Assembly Constrain.
Each point have 'Tuch/Align' constrain by 'Lock to Select Object'.

I have a tip for modifiable routing path.

You can re-define the point set from Modeling APP.
And then the Routing path will be changed by 'Lock to Select Object' and Align constrain.
(Actually, the best practices may according to how to create the point set.)


 Sunkap Ahn, Senior Support Engineer


logo