Cancel
Showing results for 
Search instead for 
Did you mean: 

Edit Object Colour conjunction with Face Rule

Phenom
Phenom

Is it possible to use “Edit Object Colour” command in conjunction with Face Rule?

(Without additional steps like Group Faces please)

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

6 REPLIES 6

Re: Edit Object Colour conjunction with Face Rule

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"Is it possible to use “Edit Object Colour” command in conjunction with Face Rule?"

 

Unfortunately, not really. However, a user on eng-tips (CNSZU) posted a journal that allows you to select tangent faces when editing object color.

 

http://www.eng-tips.com/viewthread.cfm?qid=359924

Re: Edit Object Colour conjunction with Face Rule

Phenom
Phenom

Lame!  Another ER!

 

Thanks cowski1 for sharing a workaround. I will try that route.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Edit Object Colour conjunction with Face Rule

Phenom
Phenom

Cowski1, When running that Jounal, I get this error:

mf_fce_rule_20160928.PNGJournal: Colour Face Rule.

Any idea?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Edit Object Colour conjunction with Face Rule

Phenom
Phenom

IR Description: NX: Edit Object Color conjunction with Face Rule  

Dear Customer, 

Your recent call to the Global Technical Access Center, Incident Report (IR)Number 7820371 opened on 28-SEP-2016, has been researched by our GTACsoftware engineers. They have determined that this issue should be  reviewed for possible enhancement to the current software functionality.  

This IR was converted into an enhancement request (ER) on 28-SEP-2016and is now referenced as ER Number 7820371. It is OPEN for review at this time. 

You may view the status of this report through the Create or Update an IR optionon our GTAC Support web page at http://www.siemens.com/gtac. Select the Createor Update an IR option. This tool requires a WebKey username and password. Onceyou are logged into the QTAC tool, select the Search option from the toolbar. 

Thank you for contacting the Global Technical Access Center. 

Sincerely, 

The Global Technical Access Center Team

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Edit Object Colour conjunction with Face Rule

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
That's odd. I got it to work in NX10.0.3. All I had to do was replace the path to the dlx file on line 25 in the vb script:
Public Shared JournalDirectory As String = "C:"

I tested using the instructions on eng-tips and using "Menu > Tools > Journal > Play".
Did you edit any of the content of the vb script other than the path to the dlx file?
Ben

Re: Edit Object Colour conjunction with Face Rule

Phenom
Phenom

Thanks Ben for verifing. I've missed a step: to show the Journal path.

 

It's working now. I should go back to Eng-tips and give a star to CNSZU .

 

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW