Cancel
Showing results for 
Search instead for 
Did you mean: 

Edit sketch in Task Environment

Pioneer
Pioneer

Hi everyone,

 

I seem to have gotten the hang of sketching in Task Environment.
What bothers me however is when I edit my sketch - it goes into Direct Sketching. This means all projections are outside the sketch, etc. Can I change this?

 

Thanks.

SRLSR

6 REPLIES

Re: Edit sketch in Task Environment

Phenom
Phenom

Locally: preferences>modeling>edit>.....

Overall: file>utilities>customer default>modeling>general>miscellaneous.....

 

see images (NX9)

 

Ciao

 

Cesare

Re: Edit sketch in Task Environment

Creator
Creator

Got to The Modeling preferences and select the Edit Tab. Then change "Edit Sketch Action" to Task Environemnt.

Re: Edit sketch in Task Environment

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Like Cesare and Elljay are saying is that you can set the change to open in task environment.


But what do you mean by projections are outside the sketch?
are you meaning projected curves or something else.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Edit sketch in Task Environment

Pioneer
Pioneer

Yes, sometimes they are seen as separate features, which i don't understand.

Re: Edit sketch in Task Environment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

When working in the sketch environment, there is a "project curve" command, these curves will be created as sketch curves and live in the sketch. There is also a "project curve" command that you can use outside of the sketch; these curves can be created as associative/unassociative and will not be part of a sketch (the associative option will create a project curve feature in your model tree). Perhaps you have one or more of the non-sketch "project curve" features in your model?

Re: Edit sketch in Task Environment

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Cowski, thats was also what i was thinking about.

 

some people use the feature projected curves when they don't need the curves for a sketch or get

non-associative curves to extrude a solid from.

It's also possible to use booth methods trough each other.

 

only when you need the projected curves in a sketch then i preferred to use the projected curve command in the sketcher.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions