03-10-2017 09:44 AM
Yesterday I modified the modeling template to have a different background color (I prefer blue over grey). I thought it was working fine, but this morning I discovered that if I edit a sketch "with rollback" it reverts back to the grey background. If I edit (without rollback) I get the blue background. So there must be another setting change that I missed. Where is that? Thanks for the help!
Solved! Go to Solution.
03-10-2017 10:19 AM
In the sketch preferences, the options for the background are "plain" or "inherit color"; the description for "inherit" says that it will inherit the background color of the previous application. It sounds like you want the "inherit" option.
03-10-2017 10:38 AM