Cancel
Showing results for 
Search instead for 
Did you mean: 

Editing bolt circle diameter with Synchronous

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everyone!

I realised that I don't know whether it is possible or not to edit bolt circle diameter with Synchronous technology. Say, if there are six hold lying on 100 mm diameter, and I want them to lie on 120 mm diameter. There is a workaround I am aware of - to delete 5 of the holes, then move remaining hole, then re-create pattern using Pattern face. But is it possible to do this directly with Synchronous, without deleting the holes - just recongise them as a pattern and shift altogether. NX10.

2 REPLIES 2

Re: Editing bolt circle diameter with Synchronous

Siemens Phenom Siemens Phenom
Siemens Phenom

Seems to be only achievable by the work around.

Re: Editing bolt circle diameter with Synchronous

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Existing ER 6206681.

Regards, Ben