Cancel
Showing results for 
Search instead for 
Did you mean: 

Enable Snap point

Creator
Creator

Hi

When I open or create new part. I would like to use "snap point on face" as defualt.

How to enable "snap point on face" as defualt and all point command?

Thank you  

NX10.0.2 MP02

Windows 7

1 REPLY 1

Re: Enable Snap point

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make sure that dialog memory is enabled (user defaults -> Gateway -> user interface -> general -> save dialog memory between sessions); restart NX if necessary. Now start the point command, set the snap options as desired, create a point and OK the dialog. The snap settings will be saved and applied the next time you use the point command.