Cancel
Showing results for 
Search instead for 
Did you mean: 

Enforce piece part

Genius
Genius

Is it possible to see if a part is enforced as piece as atribute, so you can publish it to teamcenter?

3 REPLIES

Re: Enforce piece part

Siemens Phenom Siemens Phenom
Siemens Phenom

Its not clear what do you exactly want, Could you please mention some more details with example so that it would be easy to help you. Smiley Happy

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Enforce piece part

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
There does not appear to be an exposed attribute when a part has been set to "Enforced Piece Part". Please contact GTAC and submit a new ER. In the interim you could manually set a part attribute in the NX part and map that to TC.

Regards, Ben

Re: Enforce piece part

Genius
Genius

Thank you Ben, I think you are right, I will ask for an ER.

 

Ganesh, I usually set some parts as enforced piece in order to avoid move another component inside them by mistake. I do that in the enforced part menu that can be reached by utilities menu. I would like to view if a part is enforced as piece in a way that can be exposed to Teamcenter so I can create reports looking for some kind of items that should be enforced as piece and they are not, so I can "repair" them.