Cancel
Showing results for 
Search instead for 
Did you mean: 

Enforcing Site-level customer defaults

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello everyone!

Site-level defaults are defined, all necessary variables are set. But user's machine is launched with User-level defaults and drafting standard in drafting files is subsequently taken from the User-level setting, while Site-level settings and corresponding drafting standard is required. How can Site-level settings be enforced upon NX launch?

3 REPLIES

Re: Enforcing Site-level customer defaults

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have the desired options been locked at the site level? If not, the user defined options can (and will) override them.

Re: Enforcing Site-level customer defaults

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Thanks, I will check that.

Re: Enforcing Site-level customer defaults

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And...

Once you lock them at the site level, the user level settings will (likely) cause a warning message during NX startup.

To get rid of the message, IIRC:

- look in the NX log file (File -> Help -> Log file) to see what settings are causing the issue

- IIRC, you can't use customer defaults to delete them (I may be wrong).  If you can't, you have to manually delete them from the DPV file (assuming you want to save the other user level settings) - open DPV n a text editor, find & delete the appropriate lines.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled