05-21-2015 11:06 AM
NX 9.0.3.4
Is there an environment variable to point all users to a network location of the CAD reuse libraries instead of X:\Siemens\NX 9.0\NXPARTS?
Solved! Go to Solution.
05-21-2015 11:17 AM
There is a spot in the customer defaults file to point to reuse area that everyone would need access to. It is in the Gateway -> Reuse Section on the General tab.
Hope this helps.
Scott
05-21-2015 11:59 AM
Thanks Scott, that's it, I searched everywhere except the customer defaults..............JD