Cancel
Showing results for 
Search instead for 
Did you mean: 

Error Exporting JT File From NX

Valued Contributor
Valued Contributor

In NX10 when I try to export a JT file I am receiving the following error message:

"Default configuration file tessUG.config is not found in C:\Program Files\Siemens\NX 10.0\pvtrans"

 

Has anyone else seen this before or know what it is referring to?

Michael Pinto | Designer
NX11|Windows 10 Enterprise 64bit|HP Z-Book Studio G3 Workstation|Intel XEON E3-1505M|32GB Ram|Nvidia Quadro M1000m w/4GB
1 REPLY

Re: Error Exporting JT File From NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is that file in the folder specified?

If not, did someone rename it?

Is there a different .config file in the folder?

 

Is the file missing on only 1 PC, or on all of them?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled