Cancel
Showing results for 
Search instead for 
Did you mean: 

Error: One or more bodies are suspected of being corrupt

Experimenter
Experimenter

Hey everyone,

First post! Yay. Been using NX for a couple years now. Started with NX7 then NX9 now NX10.

 

Today I got an error message when working in one of my control stucture files what read:

"Error: One or more bodies are suspected of being corrupt"

 

Is there a tool in NX to help locate corrupted bodies or anyway to help narrow my search?

 

Thanks,

Lewis

3 REPLIES

Re: Error: One or more bodies are suspected of being corrupt

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Turbine_Design,

 

What commands were you using leading up to the error being raised?

Are you using the newest maintenance release of NX10?

You should consider contacting GTAC for a quick analysis of this error.

 

Regards, Ben

Re: Error: One or more bodies are suspected of being corrupt

Experimenter
Experimenter

@BenBroad,

These files have given me issues since i first started working on them about a year ago. They take a very long time to open at times and some other users cant open them at all. The files were working great to update sketches and wave links them all i did was shade the objects and it gave me the error.

 

I am using 10.0.3 MP16, not sure if MP16 is the newest.

 

Lewis

 

Re: Error: One or more bodies are suspected of being corrupt

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
If rendering is raising the error then see if anything is flagged when you execute Examine Geometry against the parts. The latest patch for NX10.0.3 is MP19.

Regards, Ben