Cancel
Showing results for 
Search instead for 
Did you mean: 

Error on printing for the second time

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

NX10 I have this problem: when I print (File->Print) I can only print once; if I try to print a second screenshot or drawing  I get "Internal error memory acces violation", or Nx crashes. In both cases I have to restart NX. With NX9 everything worked, I dont't understand if it is a  "printer side" problem or "NX side" problem.

I attach the log file, thank you for any good tip

Lau

6 REPLIES

Re: Error on printing for the second time

Experimenter
Experimenter

Hi,

 

If you have access to GTAC you can find the solution there.

 

IR Number:8278071

 

 

 

Re: Error on printing for the second time

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

thank you very much Smiley Happy, I will try and download the patch as suggested

Re: Error on printing for the second time

Experimenter
Experimenter

Hi, what was the patch you used to fix this problem?

 

Thanks!

Re: Error on printing for the second time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Guessing...

 

Did you go to

https://solutions.industrysoftware.automation.siemens.com/

 

If not, go there.  You should be able to use the same username/passwrod as here (if you are using a webkey account to get in here)

 

Search on the indicated IR number

Follow the instructions

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Error on printing for the second time

Experimenter
Experimenter

Got it, thanks!

Re: Error on printing for the second time

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

sorry for not answering, I have been off line for a while. But I see you have solved, thank to Ken!