Cancel
Showing results for 
Search instead for 
Did you mean: 

Error opening a .PRT ? Memory access violation ?

Genius
Genius

Hello

Error opening .PRT. Memory access violation ?

  • Failed to load part file when responding to request from another application ?

error open file.png

8 REPLIES 8

Re: Error opening a .PRT ? Memory access violation ?

Genius
Genius

Seems I can only open:

  • The model file
  • or
  • The drawing file at the same time ? (Both can't be open at the same time)

+ Can't update the drawing on this model ?

  •  "A deleted or invalid class id was used"

ERROR UPDATING.png

Re: Error opening a .PRT ? Memory access violation ?

Genius
Genius
Deleted drawing file and created a new drawing. Now works.
-> Old drawing corrupted ?

Re: Error opening a .PRT ? Memory access violation ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @12131444,

 

It does look like the drawing is corruted.

 

2 options you could also have tried:

 

1) Open the drawing structure only, and save it again.

2) Do a part cleanup on the drawing and part file. This might solve any issues that are found.

 

Might help you the next time.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Error opening a .PRT ? Memory access violation ?

Honored Contributor
Honored Contributor

Was the flat pattern replaced, in the model?  I've had issues where the flat pattern was deleted, and a new one created in the model, and then the drawing freaks out, because the data is now gone.  I've had to open the drawing 'structure only', delete the flat pattern view, and then add the new flat pattern.

 

Might be related, may not.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Error opening a .PRT ? Memory access violation ?

Genius
Genius

Yep. That was the case.

Original Flat-Pattern was deleted. Smiley Very Happy

  • What exactly means "Open drawing structure only" ?

Re: Error opening a .PRT ? Memory access violation ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @12131444,

 

It simply means, you open the drawing, but without loading the parts. So you are only loading the structure of the assembly (in case of a drawing, the top assy is the drawing, with a Part underneath it).

 

Check this box, on opening:Open structure only.png

 

And it will load the drawing like this:

Structure only.png

This will give you the oportunity to avoid the error, trow away the flat pattern, and now load the part again, and place the new flat pattern.

 

Hope this helps.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Error opening a .PRT ? Memory access violation ?

Genius
Genius

Any easy way to replace the Flat-Pattern so it refreshes/updates the old one without errors ?

  • when old one deleted and new one added or so...
  • Now I have to make measures and all that again (when adding new base view flat-pattern)

Re: Error opening a .PRT ? Memory access violation ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @12131444,

 

When updating an flat pattern, all should go OK, automatically. Only in this case, it seems like you have deleted the existing flat pattern, and created a new one. On the drawing it's still looking for the "old" one, which no longer exists. And the new one is not on the drawing yet.

 

I hope this clarifies it a bit?

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software