Cancel
Showing results for 
Search instead for 
Did you mean: 

Error "The input section is not valid" for imported IGES file

Valued Contributor
Valued Contributor

Hi, 

I have a problem for  imported IGES file in NX11,

I tried to extrude from curves insde the imported file,

But i got error "The input section is not valid", as picture below,

You can get the .prt in attached file,

Could anyone can help me to check the reason ?

2018-01-01_210429.png

6 REPLIES 6

Re: Error "The input section is not valid" for imported IGES file

Siemens Phenom Siemens Phenom
Siemens Phenom

A single curve is nearly half a kilometer long, tangent curve get to more than a kilometer.

Assume the units were incorrect in the iges file, or is this a large construction project?

 

Steve V

Re: Error "The input section is not valid" for imported IGES file

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

did you try to add the curves to a sketch and use then the optimize curve?


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Error "The input section is not valid" for imported IGES file

Gears Phenom Gears Phenom
Gears Phenom

Ciao @WANGHUA198211

 

As @StevenVickers says, the curves are too big. Try to scale these as I do (0.001x) and it all works!

 

Ciao

 

scale.png

Highlighted

Re: Error "The input section is not valid" for imported IGES file

Valued Contributor
Valued Contributor

Hi, Steven,

 

Thank you for your feedback,

I just exported to IGES file from ICEM CFD for HEX meshing exercise in NX.

Maybe it is unit error

Re: Error "The input section is not valid" for imported IGES file

Valued Contributor
Valued Contributor

Hi, Ruud,

 

Thank you,

I tried to project curves to sketch,

it didn't work.

Re: Error "The input section is not valid" for imported IGES file

Valued Contributor
Valued Contributor

Hi, Cesare,

 

Thank you very much for your help,

Yes, i also succeeded,

It works.