Cancel
Showing results for 
Search instead for 
Did you mean: 

Error update patch NX 11.0.2

Genius
Genius

Hello

Update patch nx-11.0.2.mp04 Error.

run_ugsupdate.exe

 

Install Failed

Error 255 from running

c:\........\nx-11.0.2.mp04\ugs_update.bat/pand1

 

Updating files in AUTOMATION_DESIGNER
Access denied
Unable to create directory
Error updating
echo was unexpected at this time

unabledir.jpgautomation designer.jpg

2 REPLIES

Re: Error update patch NX 11.0.2

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @12131444,

Do you have admin rights on that machine? Try to run the batch file with option 'Run As Administrator'.

 

Refer to the discussion of the following post.

NX 11.0.2 - Maintenance Pack 2 Announcement

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Error update patch NX 11.0.2

Genius
Genius
Yes "run as admin" worked. Thanks