Cancel
Showing results for 
Search instead for 
Did you mean: 

Error when using Patch function

Valued Contributor
Valued Contributor

I am trying to patch the ends of a piping model after capping them with bounded plane. I plan on using space finder to get an internal volume, but I get an error message saying

"Tool Sheet Edges are not close to target body or do not form a closed loop."

The other end of the piping model is capped, but it isn't patched.

 

 

1 REPLY 1

Re: Error when using Patch function

Siemens Phenom Siemens Phenom
Siemens Phenom

Try the Patch Openings command.  It is more applicable in the case you described than the Patch command.