Cancel
Showing results for 
Search instead for 
Did you mean: 

Existing Point vs. Point

Genius
Genius

The same point (non-timestampe). Two occurences. Why?  Thanks!

 

ScreenClip [2].png

 

within Datum Plane:

ScreenClip.png

 

 

3 REPLIES 3

Re: Existing Point vs. Point

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
That is odd - I reproduced it. I'd suggest opening an IR with GTAC so they can have development take a look at it.

Regards, Ben

Re: Existing Point vs. Point

Siemens Phenom Siemens Phenom
Siemens Phenom

This behavior has been there since point snapping was introduced. It seems redundant but I'm sure it is this way by design. One is for the point object, the other is for the type of point snapping that's being done. If you toggle off the 'Existing Point' option in the selection bar, then quick pick will only show one object; the point object. In the datum plane by 3 points case, because the system is filtering selection to points or routing objects, you may turn off all point snapping and still be able to construct the plane by selecting the point objects.

Regards,
Abe

Re: Existing Point vs. Point

Genius
Genius

Hi @Abeinjapan, your explanation is very clear. Thanks!

 

Hi @BenBroad, thanks for your reply!