Cancel
Showing results for 
Search instead for 
Did you mean: 

Exit sketch in model environment?

Valued Contributor
Valued Contributor

How do you exit a sketch while in the model enviroment, without keeping any changes that were made? Surely there must be a way, but I can't seem to find it.

 

Thanks!

Pat 

5 REPLIES

Re: Exit sketch in model environment?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Exit & save changes, then Undo?

(although you might then have to wait for the model to update...twice)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Exit sketch in model environment?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you use the sketch environment, you can go to Task -> exit sketch.

I don't use "direct sketch", but I assume there is a similar option there.

Re: Exit sketch in model environment?

Valued Contributor
Valued Contributor

Thanks for the replies.

 

Clicking "Finish Sketch" then Undo does work, but I was hoping for something more direct, lilke "Exit Sketch," which doesn't appear to be available in the modeling environment.  Not sure why.  I guess I'll do the other for now.

Re: Exit sketch in model environment?

Siemens Phenom Siemens Phenom
Siemens Phenom

As @cowski1 mentioned, you can use Sketch in Task Environment and use Task > Exit Sketch to discard the changes.

 

If you have a sketch present already, Just use Edit with Rollback..Do the changes and use Task >Exit Sketch to discard the changes. If you use Edit option you have to end up with Finish Sketch option. Task tab will available only if you use Edit with Rollback.

 

Sketch_exit.PNG

 

 

Re: Exit sketch in model environment?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

In the sketch task environment you can choose exit from the file menu.

 

In direct sketch, where you sketch directly in the modleing environment you can use undo (just like when you are creating and editing features). You can undo any operation you did, even entering the sketch. Just go back in time. The undo menu (under the undo button) will allow you to undo multiple actions in a single operation. Just choose "enter direct sketch".  

 

Regards, **bleep**