11-19-2015 11:04 AM
Hello folks !
I was wondering, if there is a way to export the results from following performed analysis into some 3D format (preferably JT / 3D PDF) from with in NX.
1) Check Wall Thickness
2) Draft Analysis
3) Local Radius Analysis.
Appreciate some pointers,
Cheers !
11-19-2015 05:18 PM
For the Draft you can change your surfaces of your model to certain colors using the molded part valadation tool. Look under the face tab to change the color on your drafted surfaces. I do not know if you can do the same with the Wall Thickness. Once you get these surface colors you can export JT file of your model. The color of your surfaces should stay once you export to JT file. Now if you are using a 3D pdf you may need to export out a step using the ap214 standard to keep the surface colors. I do not have much experience with radii analysis. I would also have you look into a addon called DFMPRO. It has some great tools for checking your models also.
12-02-2015 12:28 PM
Thank you for the great tips ! Yes, we are also considering DFM Pro for NX.