Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Export NX 10 Role

Experimenter
Experimenter

Hi.

Can anyone help me with the role function in NX 10? - Can it be true, that I can't export my role? I know that it has been possible in the past, but I can't find the command/function to export my Role in NX 10. I can't see in NX where the role file refer to now, soo I can't even find the .mtx file and just copy it... 

 

Thanks in advance.

5 REPLIES 5

Re: Export NX 10 Role

Siemens Phenom Siemens Phenom
Siemens Phenom
Role files are normally stored in the following location:

C:\Users\username\AppData\Local\Siemens\NXXX\user.mtx

Re: Export NX 10 Role

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Normally I just MB3-click in a blank area of the "roles" resource bar -> "New User Role"

 

Or is that not what you are trying to do?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Export NX 10 Role

Experimenter
Experimenter

Rony's answer was the solution. I just had to find my role and copy it to a new colleague who starts tomorrow - then it's easier to help him :-) I couldn't see the MyRole.mtx file under C\user\username\App etc. but then I tried to use the search bar where I searched for ".mtx", and then it popped up.

Re: Export NX 10 Role

Legend
Legend

Hi Dennis,

 

You can export your interface Role in NX10.0 following the steps below.

 

1 - Menu > Preferences > User Interface.

1.png

 

2 - In the User Interface Preferences dialog box, click New Role.

2.png

Jean Marcel
PLMPRO
www.plmpro.com.br

Re: Export NX 10 Role

Experimenter
Experimenter

Arhh okay, I think that is a bit misunderstanding :-) I thought that it would reset everything then. Thanks for your reply Jean.