Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Pioneer
Pioneer

Hello,

I am trying to export a PDF with some Shaded Geometry in it, but the output file contains only wireframe geometry.

I am using the same settings as usually, and the same file was exporting properly some days ago. I can't figure out what is making my shaded views show as wireframe. The PRINT command also shows only wireframe.

The export settings are the following:

Captura.JPG

 

Exporting other drawings with different geometry works properly. Has this bug also happened to anybody?

The file I am trying to export is really heavy, is there a processing limit that stops NX from exporting shaded views?

 

Thanks in advance for your help.

MSV


MSV
NX 9.0.3.4
NX 11.0.0.33
17 REPLIES 17

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

The only way I'm aware of is to add a shaded view in Drafting and export the drawing as a PDF.

Regards, Ben

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Pioneer
Pioneer
Hi Ben,
Thanks for your reply.

The link you posted seems to be broken.
The weird thing is that when NX exports/prints the drafting, the shaded views appear without any shading (just the wireframe).

Regards

MSV
NX 9.0.3.4
NX 11.0.0.33

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Pioneer
Pioneer
Yep, that is what I've been doing all the time.
The problem is that with this file (and only this file), this is not working. Even though the shading is set to "Fully Shaded" the exported PDF shows only wireframe geometry.

Thanks for your answers.

MSV
NX 9.0.3.4
NX 11.0.0.33

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Can you provide the file (either here or have GTAC look at it)?

Regards, Ben

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We've had various issues with shaded views in pdf files. The main one for us is if the view borders overlap (just the borders, not the actual geometry in the view); in this case the geometry in one or both views will come out as wireframe. The drawing will look OK on the screen, but will not plot or export to pdf correctly.

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

You can predict the result by selecting 'File > Plot', expand the Actions block and choose Advanced Plot. On the Printer page you'll see an option at the bottom called 'CGM Viewer'. This will open a new dialog showing what will be sent to the printer/plotter/PDF.

@cowski1 could be on to something with the overlapping view borders. The other thread started by @guga50 reporting that a shaded view did not plot at 1:1 seems to be because the view borders extend beyond the drawing border. Once the view boundary was edited so the view boundary falls inside the drawing border, the PDF exported.

Regards, Ben

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Pioneer
Pioneer

Hi,

Finally I could export it properly. There has to be some misconfiguration/bug with the sheet.

I created a new sheet and copied all the views in it. Copying the whole sheet did not worked, but moving the views did.

 

Thanks for your help.

Regards.


MSV
NX 9.0.3.4
NX 11.0.0.33

Re: Export PDF: Shaded Geometry as Wireframe even if checkbox not selected

Experimenter
Experimenter

Anyone know how to solve the issue that cowski1 is referring to?

I am having the same issue. I have a section view in NX drafting but when I export to PDF, the pdf shows what appears to be geometry that was ommitted from the section view in NX. Any help would be greatly appreciated.