Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Export PDF out of TC with a workflow

Experimenter
Experimenter

I am trying to export a PDF dataset that is already in TC out with a workflow.  I want to add this to the end of a release workflow.  Export the PDF to a specified folder on the network.  I need help figuring out what Hanldlers to use and how to make this happen.  I am trying to teach myself this workflow programming and am stumbling thru it.  So I am going to ask a bunch of stupid questions, so bare with me. haha.

 

TC10(10.1.6.1(20160515.00)) 64-bit

16 REPLIES 16

Re: Export PDF out of TC with a workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

I do this with the EPM-run-external-command handler.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Export PDF out of TC with a workflow

Legend
Legend

Hi Larry,

 

Is that handler still works in 10.1.7.1?

 

I  see no files were exported from the above handler, Do you have any suggestions?

 

image.pngimage.pngimage.png

Regards
Rafa

Re: Export PDF out of TC with a workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

Since it still exists in Tc11.3, I have to assume that it still exists and works in later SPs of Tc10.1 including 10.1.7


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Export PDF out of TC with a workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

If you want syntax examples, download my 2009 PLMWorld Conference slide deck at

Creating PDF Files Using OOTB Tools

 


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Export PDF out of TC with a workflow

Legend
Legend

I did follow your syntax, but still have no luck on the export.

 

When I checked syslog it says "No env vars found.  Leaving original value" (attached syslog)

 

image.png

image.png

Regards
Rafa

Re: Export PDF out of TC with a workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

You're missing the most import agrument; the script you're going to input these files into. The handler requires a program to run to use your list of exported files as inputs.

 


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Export PDF out of TC with a workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

You're also missing the parenthesis around (ItemRevision) for your target.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Export PDF out of TC with a workflow

Legend
Legend

Thanks Larry,

 

Yes, works fine in 2-tier now but having problem with 4-tier!

 

Folder  \\WFIS1\TestDrwaings\DataExportLogs was shared to everyone!! Not sure if this works in 4-tier? 

 error.png

Regards
Rafa

Re: Export PDF out of TC with a workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

It works fine in 4 tier. I know because that's what we use too.  If it works in 2 tier but not in 4tier, it's most likely a permission issue on the file share.  Ensure that the service account running the service manager has the same access as the acccount you're using for 2 tier.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,