Cancel
Showing results for 
Search instead for 
Did you mean: 

Export .dwg file with .jpg in NX

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi everyone,

 

I insert .jpg file to draft in NX and then I export it  to .dwg. When I try open new .dwg file in NX I can not see jpg. I just see the title block and nothing more. Pls check attachment. In solidEdge it is working well so I hope it is possible in NX as well. There is anyone who is able to help me?

 

dwgNX.pngjpgnx.png

 

 

3 REPLIES

Re: Export .dwg file with .jpg in NX

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @lukipap,

 

The functionality you are looking for is not currently supported.  Enhancement request ER 6890616 has already been submitted asking for the ability to include images when using the DXF/DWG translator.  Shaded views are also not supported.  If you must have a DWG consider exporting a CGM using the Advanced Plot command and then using a CGM -> DWG converter.  Export PDF would also work.

 

Regards, Ben

Re: Export .dwg file with .jpg in NX

Pioneer
Pioneer
Hi, Ben, I'm working in NX11, is the functionality discussed in this thread supported yet? I'm exporting to dwg for a client, and everything shows except our company logo... My boss is not impressed. Smiley Sad Smiley Sad Smiley Sad Thanx.

Ed

Re: Export .dwg file with .jpg in NX

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @lonesome-joe,

 

Unfortunately it does not appear that the ER has been implemented yet.  Please consider opening an IR with GTAC to have yourself added to the ER.

I did find one IR that mentioning that starting with NX 11 the image was exported along with the DXF/DWG, as a separate file, and that the image is positioned correctly in the drawing when using AutoCAD 2017.

 

Regards, Ben