Cancel
Showing results for 
Search instead for 
Did you mean: 

Export image and edit section PROBLEM

A few days ago I sew a meme on facebook that say

"we have found a bug

we have solved bug

now we have two bugs"

 

it's writed for Bungie software house but it's work also for Siemens.

 

I want to export an image of a part sectioned with edit section and section curve preview active.

Before 12.0.2.9

click Edit Section

click Show Section curve preview

click Export image

and I can save image like example 1 attacched

 

After 12.0.2.9

click Edit section

click Show Section curve preview

click Export image

and NX close command Edit section, so it's impossible to have a sectioned image whit curve active, I must to copy to clipboard and attach in photoshop for have the same image.

 

If these are the advantages of maintenance I think it's the last year that I pay for it!!

 

 

2 REPLIES 2

Re: Export image and edit section PROBLEM

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Speziali_Bruno,

Reason that you do not see the behaviour you have described may be because of enhancement Capturing an image of graphics window enhancements in NX 12.0.1

 

With this enhancement different export image options are combined in single command/dialog.

 

When 'Edit Section" is used then section will be created under 'Sections' folder node in the assembly navigator. You can toggle on/off this section and use the new 'Export Image' command in same way to capture section with curves.

Section_node.jpg

 

Re: Export image and edit section PROBLEM

Thanks @GaneshKadole,

Siemens give me back the same quick solution, but they agree that it's a bug.

Anyway I'm very disappointed from Siemens, I think they are getting worse.