Cancel
Showing results for 
Search instead for 
Did you mean: 

Exporting Convergent bodies as parasolid or STP files?

Experimenter
Experimenter

Is it possible to export a convergent body as a parasolid or STP file?  It can be exported as an .STL

 

Any feedback would be appreciated, thank you.

2 REPLIES 2
Highlighted

Re: Exporting Convergent bodies as parasolid or STP files?

Siemens Phenom Siemens Phenom
Siemens Phenom

@David53

This is not possible. Convergent bodies are not b-rep bodies, they are a new type of object called a Parasolid Mesh which is basically facet based. Export to Parasolid or STP require a b-rep solid or sheet body.

Regards,
Abe

Re: Exporting Convergent bodies as parasolid or STP files?

Phenom
Phenom

@David53

I had the same question not so long ago.

File an ER. There is anexisting ER for this; ER 8986996. Add your name to it.

Maybe something will happen faster.

Huysmans Metalen n.v.
2x NX1867 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend