Cancel
Showing results for 
Search instead for 
Did you mean: 

ExpresReview and NX11

Legend
Legend

Is it possible to create a package file in NX 11.0.1

 

I can't find it...

Help can't find it. Says it is available in the "Gateway Application"

 

Was there and worked in NX10

 

Bueller... Bueller?

 

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

5 REPLIES

Re: ExpresReview and NX11

Gears Phenom Gears Phenom
Gears Phenom

Also says only available in native NX, if Xpressreview is installed.  I wonder if installation order plays a role?  We are Teamcenter managed, so we don't use package files, just export JT's.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: ExpresReview and NX11

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Try looking under "Menu > File > Send to Package File", or using the Command Finder. I just installed XpresReview 10.1.3 update 3 and restarted NX11.0.1 - the option is in the menu. Note that the command was removed from NX Manager because it does not work in that environment.

Regards, Ben

Re: ExpresReview and NX11

Siemens Phenom Siemens Phenom
Siemens Phenom

This one for XpressReview

 

xpress.png

 

EDIT:

Seems that while posting this @DaveK@BenBroad already posted comments. Xpressreview is needed to use this functionality.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: ExpresReview and NX11

Legend
Legend

I see... need to install it. I think before 11 you used to see the "create package file" option before it was installed.

 

Next problem is reading the readme file it states not compatible with Windows10

 

That's a problem... Paul S.

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: ExpresReview and NX11

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Ignore the readme, it works fine on Windows 10.

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2