Cancel
Showing results for 
Search instead for 
Did you mean: 

Expression, Vector type

Gears Phenom Gears Phenom
Gears Phenom

In NX9, we could unitize a vector expression, by selecting a line, face, etc.

NX9.jpg

In NX11 it appears it wants me to type something, and the only thing I can get it to find, are other expression names?   How is this supposed to work?  Help files are really lacking here.

NX11.jpg

-Dave
NX 11 | Teamcenter 11 | Windows 10
8 REPLIES

Re: Expression, Vector type

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Hi Dave,

Please open an IR with GTAC so that development can review this.

Thanks, Ben

Re: Expression, Vector type

Gears Phenom Gears Phenom
Gears Phenom

Done.  IR  8890935 if you want to play along.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Expression, Vector type

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Thank you. It is now in the hands of development.

Regards, Ben

Re: Expression, Vector type

Siemens Phenom Siemens Phenom
Siemens Phenom

Nice catch Dave... infact it is working fine in NX10 also ..so i presume issue has something to do with NX11 only.

Best Regards

Kapil

Re: Expression, Vector type

Siemens Phenom Siemens Phenom
Siemens Phenom

Dave --

 

A little update on this one.

 

Talking with the developer, it appears that when we created the new Expressions dialog in NX 11, we ran into some limitations in our dialog system, and these limitations (regarding the depth to which menus can be launched from each other) precipitated the change.

 

There's apparently a way to "fix" this, but it's going to take a fairly large project.  So please hang tight.  I'm aware of this one now.  Thanks for pointing it out.

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Expression, Vector type

Gears Phenom Gears Phenom
Gears Phenom

@TaylorAnderson thanks for the update.

 

The reason I discovered this, is Shirish More at Siemens is going to help us with some import/export of named points, with coordinate and vector data.  While i was going to create a demo file, I realized I could not create the unitized vector data.

 

If this is going to be a longer term project, do you have any suggestions on other methods to create vector data, for export/import via xml?

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Expression, Vector type

Siemens Phenom Siemens Phenom
Siemens Phenom

Dave --

 

Let's work this offline with Shirish, if that's okay.  (I see you've already sent me an email.)

 

Thanks!

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Expression, Vector type

Gears Phenom Gears Phenom
Gears Phenom
10-4!
-Dave
NX 11 | Teamcenter 11 | Windows 10