Cancel
Showing results for 
Search instead for 
Did you mean: 

Expression keeps disapearing

Experimenter
Experimenter

I have been working with string and logic expressions. The string expression changes text and a value, depending on the length. The text is an extruded cut into the model.  The logic expression I am having a problem with is used as a value for P5. I set P5 = to the variable name of "printext".  I have created "printext" as a length and a constant, neither works more than once. "objlen" is the controlling variable. I can change it once and "printext" works. Then the value for P5 returns to a number, and doesn't work correctly after that. I have attached a jpeg file of the expressions. I am having trouble attaching the prt file. If someone is interested please notify me and I will try to email it.

10 REPLIES

Re: Expression keeps disapearing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

ZIP your part file, then you can attach it.

A free (speech and beer) option to do this is 7 zip

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Expression keeps disapearing

Experimenter
Experimenter

Here it is.

Re: Expression keeps disapearing

Siemens Phenom Siemens Phenom
Siemens Phenom

Interesting...

 

The Text(3) feature that controls the Length expression (p5) does not appear to be correctly storing the expression formula here.

 

I would suggest submitting an IR for this against the Text feature, specifically.  Development can then look at whether they think this is a PR or an ER.  I would lean toward a PR, personally.  :-)

 

Good catch!  Thanks!

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Expression keeps disapearing

Experimenter
Experimenter

I sent the file to Siemens as an "IR". They are presently working on the problem.

Re: Expression keeps disapearing

Siemens Phenom Siemens Phenom
Siemens Phenom

Thanks, jazzer10.  Can you send me the IR number?  I'd love to follow up.

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Expression keeps disapearing

Experimenter
Experimenter
IR 9054677

Sent from my iPhone

Re: Expression keeps disapearing

Siemens Phenom Siemens Phenom
Siemens Phenom

Thanks!

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Expression keeps disapearing

Valued Contributor
Valued Contributor

HI Taylor Anderson

I was wondering if you have heard anything about my IR 9054677 ?  I don't know how to check with GTAC about it.

Thanks

Steve

Re: Expression keeps disapearing

Valued Contributor
Valued Contributor

Hi Taylor

Never mind about the last reply, I have been contacted by GTAC.