Cancel
Showing results for 
Search instead for 
Did you mean: 

Expressions driven by arrangements

Creator
Creator

Is there a way to influence the value of an expression by means of arrangements?

9 REPLIES 9

Re: Expressions driven by arrangements

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is currently (as of NX 9, at least) no way to link expressions and arrangements.

Re: Expressions driven by arrangements

Creator
Creator

Oke, it sounds like you are pretty sure. I was already afraid of that.

Thanks for your response anyway.

Re: Expressions driven by arrangements

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Not directly, no. If you're willing to use "Update for External Change" you can get creative.

For example, if you have a distance constraint between two components, that has a unique value for each arrangement, you could create a measurement expression between the components (at the assembly level) whose value drives other interpart expressions using conditional expressions. The caveat is that measurement expressions do not automatically update when arrangements are changed (ER 7278506), hence the need to use Update for External Change.

Regards, Ben

Re: Expressions driven by arrangements

Phenom
Phenom

take a look here.  It is a good work around

 

http://www.eng-tips.com/viewthread.cfm?qid=238760

Re: Expressions driven by arrangements

Creator
Creator

Thanks for your advice Ben. I already tried to use the measurement expression but indeed this value didn't update after switching between the arrangements. However, I wasn't aware of the option "Update for external change". This option works well if you do the update manually, but is there a way to changed the default NX settings so that the update will be done automaticly after a change of a arrangement?

Re: Expressions driven by arrangements

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

... is there a way to changed the default NX settings so that the update will be done automaticly after a change of a arrangement?

Unfortunately not and unfortunately there aren't any NX Open calls to perform an Update for External Change (ER 6771744), so a user exit (or post action) would not work either.

 

Regards, Ben

Re: Expressions driven by arrangements

Siemens Phenom Siemens Phenom
Siemens Phenom

Ben --

 

There's a KF function in pts_func.dfa (used for immediate updates in Product Template Studio) with an accompanying C function that can initiate an Update for External Change:

 

Defun: %ug_updateForExternalChange(Boolean $spreadsheet_only)
@{ CFunc("KF_update_for_external_change", "kfdfun"); } Boolean;

 

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Expressions driven by arrangements

Creator
Creator

Hello Taylor,

 

To be honest your remark is a bit too technical for me. Is that something we can use in our company as well? And after using it, is there an automatically update possible?

If so, I can discuss your remark with our NX/TeamCenter department.

 

Regards,

 

Joost

Re: Expressions driven by arrangements

Siemens Phenom Siemens Phenom
Siemens Phenom

Joost --

 

There is really not an easy way to have Arrangements influence Expressions today. 

 

The "Update for External Change" method above using a measurement is probably the best workaround that doesn't involve some touchy programming.

 

Allowing the changing of an arrangement to trigger a modeling update would be a good ER for the Assemblies team.

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com