Cancel
Showing results for 
Search instead for 
Did you mean: 

Extract face

Valued Contributor
Valued Contributor

Hello, I need to use a surface from one part to build another part.

Within an assembly I make component part A my work part, extract face, cut-n-paste the extracted face into component part B then delete the extracted face from component part A. I don’t need it to be linked.

I’m fine with this method but was just curious if there might be another way?

 

Thank you!

David

TC 10.1.6.1

NX 11.0.2.7

3 REPLIES 3

Re: Extract face

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @David58 

You can use "WAVE Geomtery Linker" 

 

(view in My Videos)

Re: Extract face

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@GaneshKadole wrote:

Hi @David58 

You can use "WAVE Geomtery Linker" 

 


And if you really don't want/need the link, you can use "remove parameters" on the linked face to turn it into a dumb body.

Re: Extract face

Valued Contributor
Valued Contributor

Much better. Thank you very much!