Cancel
Showing results for 
Search instead for 
Did you mean: 

Extract unlinked geometry in an assembly

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi community,

 

Does anybody know if it is possible to extract the geometry of the components in an assembly when the assembly is work part?

The goal is to end up with the top level assembly file containing the bodies (which represent the components of the assembly).

 

Thanks!

Richard

8 REPLIES 8

Re: Extract unlinked geometry in an assembly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

wave geometry linker can do this.

  1. make the assembly work part
  2. start the wave geometry linker feature.
  3. select type ->body
  4. and then select al the bodies you need.

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Extract unlinked geometry in an assembly

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks for the quick reply Ruud but I need a method which results in having Bodies instead of Linked Bodies or Linked Bodies with a broken link.

I mean like when you export an assembly as a Step file and then open this Step file.

 

Regards,

Richard (cards Smiley Happy)

Re: Extract unlinked geometry in an assembly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if you go to the settings in the wave feature you can turn of the associative link.

then you will get broken links.

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Extract unlinked geometry in an assembly

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

But is there a way to get the regular bodies and its icon:


NX_BodyTypes.jpgNX Body types

Re: Extract unlinked geometry in an assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

@Richard_RS wrote:

But is there a way to get the regular bodies and its icon:


NX_BodyTypes.jpgNX Body types


After creating non associative linked bodies, use 'Remove Parameters' command.

Menu > Edit > Feature > Remove Parameters.

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: Extract unlinked geometry in an assembly

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks Ganesh!

 

This results in what I was looking for Smiley Happy

 

Regards,

Richard

Re: Extract unlinked geometry in an assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@GaneshKadole's method will result in unparameterized bodies as you want. A potentially faster way to get there is to use "export part" with the "remove parameters" option or exporting the component bodies to a parasolid file and importing that to your part file.

Re: Extract unlinked geometry in an assembly

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Thanks cowski1!

Your method is also giving me the wanted results.

Regards,
Richard