Cancel
Showing results for 
Search instead for 
Did you mean: 

Extrude an array of curves to the center of the cylinder

Creator
Creator

Hi everyone! I need to extrude array of curves to create sheets of the cylinder like in this photo

 

In should loke like a frame of the fuselage. Thank you!

3 REPLIES 3

Re: Extrude an array of curves to the center of the cylinder

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Did you try to select the edges with a start and end value of 0.
This Will create a sheet.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Extrude an array of curves to the center of the cylinder

Genius
Genius

If your profile is closed and planar, you can use Bounded Plane.

 

Regards André

Re: Extrude an array of curves to the center of the cylinder

Siemens Phenom Siemens Phenom
Siemens Phenom

If you ue extrude you will have to extrude for each sheet. Setting the direction is complicated because you want normal to the cylinder.

You can create a surface using law extention, this allows you create an 'extrusion' normal to a surface.

 

Regards, **bleep**