Cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to open register in PDW Die Base

Pioneer
Pioneer

Hello,

 

I have a problem with create Die Base in Progressive Die Wizard. 

When I try create new Die Base, the message appears, that failed to open register file.

I enclose pics to show my problem. 

Who has the same problem?

 

Best regards,

Jack

6 REPLIES

Re: Failed to open register in PDW Die Base

Phenom
Phenom

Did you run "Initialize Project" above Strip Design category? 

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Failed to open register in PDW Die Base

Pioneer
Pioneer

Yes, I try create Die Base after initializing project.

 

 

Re: Failed to open register in PDW Die Base

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Jack1,

 

You need to download the Progressive Die Wizard data and database update files, and install them per the README in the same location:

 

The files can be downloaded here:

https://download.industrysoftware.automation.siemens.com/

Browse (or filter) to NX using the menu of products on the left of the page and then expand the folders:
Product Updates > Progressive-die-wizard > Nx10

 

Having installed the files in their correct locations, set the variable PDIEWIZARD_DIR to the pdiewizard sub-folder and restart NX.  You should no longer get the message reporting "Failed to open register file".

 

Regards, Ben

Re: Failed to open register in PDW Die Base

Experimenter
Experimenter

how to set variable. explain me in detail

Re: Failed to open register in PDW Die Base

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @0ATOM0,

 

Either set it in your NX environment file:

C:\Program Files\Siemens\NX 11.0\UGII\ugii_env.dat

Enter a new line:

 

# Override any variables here.
PIEWIZARD_DIR=<path to directory>
#

 

Or, as a Windows Environment Variable:
"Windows Start Button > Right Click "Computer" and select "Properties" > Advanced System settings > Environment Variables".  Create a new User variable with variable name "PIEWIZARD_DIR" and value "<path to the directory>".

 

Hope that helps,

Regards, Ben

 

Re: Failed to open register in PDW Die Base

Experimenter
Experimenter

thanks man.. but now when ever i give "DIE BASE" command my "project" disappear.. and unablee to select