Cancel
Showing results for 
Search instead for 
Did you mean: 

Fatal Error c000000d

Experimenter
Experimenter

I recently upgraded to NX 11, and I'm getting a reoccurring fatal error when I'm in the simulation environment. I was just putting various loads and constraints, took a break, then came back to a fatal error "Fatal error detected unable to continue Unhandled operating system exception: c000000d"

 

I'm running NX on a Surface Book with an i7 processor and an Intel(R) HD Graphics 520 chip fatal error.jpg

1 REPLY 1

Re: Fatal Error c000000d

Gears Phenom Gears Phenom
Gears Phenom

Have you installed any maintenance releases or maintenance packs?  If not, I'd try that if you're able to.  You also might get more specialized help (for simulation) in the Simcenter area rather than NX Design.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1