Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Fatal error detected unable to continue unhandled operating system exception:c0000005

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

is this an officially supported system?

If so, you should be able to report to GTAC and see if they can reproduce it.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: Fatal error detected unable to continue unhandled operating system exception:c0000005

Valued Contributor
Valued Contributor

Hello Ken

 

this is a built in graphic chip and while a session lasts NX is working fine as supposed.There is no other graphic chip on board so the reason will not be found in the switching between cards.

I suspect the reason in some kind of sleep state that is triggered by the graphics card and then NX reacts in a manner, that it crashes. no other program does that, especially no commercially available one..

 

 

 

_____________________________
Are you familiar with my product?
click here