Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature Playback in NX10.0

Pioneer
Pioneer

Hello All,

 

Could anyone tell how compatible is Playback option in NX10.0 ?

 

The reason why I'm asking is, I have a model where I have holes created with sketch and being subtracted in a inclined plane. (Modelled in NX10.0 latest patch), when I try Feature playback ,update goes till the end of model and it comes back to the pattern again and stops with extude, when I say continue (In UI), it is not solving the model as it should. (after the update I made revolve body as current feature there it is calculating only some lines ).

 

Can any one tell me what is the problem..
Some Images are attached here for reference...

1 REPLY

Re: Feature Playback in NX10.0

Siemens Legend Siemens Legend
Siemens Legend

Hi Sathya,

 

I apologize but it is very difficult to understand the actual issue. You need to either provide the part or file an issue with GTAC.

 

Best Regards

Fred