Cancel
Showing results for 
Search instead for 
Did you mean: 

Feature hiding in assembly

Creator
Creator

Hi,

I am making a coil part, where i am hiding a revolve (5) feature in the part file, After completing the part, when i adding this part in assembly file , its shows hide revolve feature. When I am doing pattern component of coil part, its shows number of hide revolve feature.

 

Please help me to hide revolve feature by a single option, i have to do many times for hiding this feature.

7 REPLIES

Re: Feature hiding in assembly

Gears Phenom Gears Phenom
Gears Phenom

Look into doing a delete body.  This should take care of any of your bodies being hidden.

Re: Feature hiding in assembly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
And otherwise you can always delete the solid from the model reference set.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Feature hiding in assembly

Creator
Creator
But i have taken project curve on that revolve feature, i can't delete that revolve.

Vinay Kumar

Re: Feature hiding in assembly

Creator
Creator
But i have taken project curve on that revolve feature, i can't delete that revolve.

Re: Feature hiding in assembly

Creator
Creator
But i have taken project curve on that revolve feature, i can't delete that revolve.

Re: Feature hiding in assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note there is a new "delete" FEATURE.

So as long as the delete is AFTER the "project curve" (in "timestamp" order), the revolve solid exists for the "project", but doesn't for the final start of the part.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Feature hiding in assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

I think it's actually "Delete Body".

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA