Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Feature parameters sketch dimensions

Pioneer
Pioneer

Hello, I’m using NX10 inside TeamCenter and trying to get dimensions from the model into the draft using “Feature Parameters.” It is currently hidden.  After a try I get this weird warning: “hidden features cannot be used for feature parameters in non-legacy views”

In NX 10 outside Teamcenter the warning changes: “The first object associativity type is invalid”

How can I get dimensions from de model into the draft?

Thanks

1 REPLY 1

Re: Feature parameters sketch dimensions

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

I get this weird warning: “hidden features cannot be used for feature parameters in non-legacy views”

In NX 10 outside Teamcenter the warning changes: “The first object associativity type is invalid”


Hi @Zoppellari,

 

Hopefully the following will be of some help:

 

1) “hidden features cannot be used for feature parameters in non-legacy views”

This happens when the feature you're attempting to inherit dimensions from (in this case your sketch) exists on a non-visible layer.

 

2) “The first object associativity type is invalid”

PR 8856133 - Reported against NX10.  This message is raised when attempting to inherit sketch dimensions from a component on to an assembly drawing sheet.  Fixed in NX11.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration