Cancel
Showing results for 
Search instead for 
Did you mean: 

File tab- drop down menu problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

The File tab drop menu changed , how can be restore? 
NX-problem.JPG

10 REPLIES

Re: File tab- drop down menu problem

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @MilenaVelcheva,

 

Your screenshots appear to be taken with a part open (left) and with no parts open (right).

 

There's nothing to restore, it just depends on the current 'state' of NX - whether parts are open in the session or not.

 

Regards, Ben

Re: File tab- drop down menu problem

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@BenBroad wrote:

Hi @MilenaVelcheva,

 

Your screenshots appear to be taken with a part open (left) and with no parts open (right).

 

There's nothing to restore, it just depends on the current 'state' of NX - whether parts are open in the session or not.

 

Regards, Ben


If that's the case, I would not expect "print" and "export" to be available. If there are no open parts, what is there to print or export?

 

And in the pic on the right, you can see the triad in the corner of the graphics screen.

 

@MilenaVelcheva, have you changed roles or done any customization recently?

Re: File tab- drop down menu problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

when i open the part is the same problem ...NX-problem1.JPG

Re: File tab- drop down menu problem

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The titlebar of the program indicates that you are in the "viewer" and not in full CAD mode.

Re: File tab- drop down menu problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

export is only parasolid missing other possibilities , thank you Ben ! 
NX-problem2.jpg

Re: File tab- drop down menu problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Ben, how i can return to CAD mode ?thank you 

Re: File tab- drop down menu problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Export is only parasolid, no other options like before ..thank you Ben!
NX-problem2.jpg

Re: File tab- drop down menu problem

Siemens Phenom Siemens Phenom
Siemens Phenom

@cowski1 is correct.  NX is in viewer mode.  Is the user double clicking a part to open NX?  I believe this might keep opening NX in "viewer" mode.  Can the user select "NX 11.0" from the Windows > Start menu (unless they're using Windows 10 - in which case they'll need to select the NX 11 tile (note NX 11.0 Viewer in each screenshot which is what is currently being used):

 

Windows 7:

 

 Screenshot - 5_30_2018 , 8_08_41 AM 002.png

 

 

Windows 10:

 

Screenshot - 5_30_2018 , 8_21_34 AM.png

 

Regards, Ben

Re: File tab- drop down menu problem

Gears Phenom Gears Phenom
Gears Phenom

Your in NX Viewer - you will not have the full dialog

John Joyce, Manufacturing Engineer,
Senior Aerospace Connecticut
www.senioraeroct.com
Production: NX11.0.2.7, Vericut 8.0.3
Development: Tcl/Tk
Testing NX12.0