Cancel
Showing results for 
Search instead for 
Did you mean: 

Files preview not working

Genius
Genius

How can I recover this?

 

Untitled_tiich7.png

 

3 REPLIES 3

Re: Files preview not working

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

Displaying part file thumbnails within the Windows Explorer requires to register a DLL. This is normally done when installing NX, but if you have two versions of NX installed, and you uninstall the older version, the registration can be removed.

 

You can re-register teh dll by executing the following command from "Windows->Start->Run" or from within a Command Prompt (you may need to adjust the path):

 

regsvr32 "C:\Program Files\Siemens\NX 9.0\UGII\ugshext.dll"

or beginning with NX11:

regsvr32 "C:\Program Files\Siemens\NX 11.0\NXBIN\ugshext.dll"

 

hope that helps,

Johannes

Re: Files preview not working

Genius
Genius

Thank you,but it's not working,it seams to be some windows issue.

 

Re: Files preview not working

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

make sure you run the program as administrator...

 

Regards,

Johannes