Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Fix multiple broken links that reference the same body

Creator
Creator

I have multiple instance of a part, call it "SOURCE.prt", in my assembly that were then position dependent wave linked into another part. Unfortunately I had to make a change to SOURCE.prt that resulted in all the linked bodies breaking. Is there a faster way of relinking the linked bodies than fixing each link individually? Each link should be connected to the same body, the only change is their position in the assembly.

 

I am using NX 8.0.2.2

 

Thank you

Dave

1 REPLY 1

Re: Fix multiple broken links that reference the same body

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @ReichDM,


Is there a faster way of relinking the linked bodies than fixing each link individually? 

Unfortunately NO.

You have to either relink individual body from the part navigator or from the Interpart Link Browser.