Cancel
Showing results for 
Search instead for 
Did you mean: 

Flat-Pattern remove bend annotations by default ?

Genius
Genius

How to

Flat-Pattern(Sheet Metal): remove bend annotations by default ?

  • Bend annotations are OK to appear in drawings.
  • Now when exporting .DXF I have to remove annotations and bends in DraftSight separately... Using a separate software to do this is labourous.

Bend annotations.png

4 REPLIES 4

Re: Flat-Pattern remove bend annotations by default ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Please refer to a raw movie below . Is this what you want?

Best Regards

Kapil

(view in My Videos)

Re: Flat-Pattern remove bend annotations by default ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you want the annotations in your drawing, but not the exported DXF, you can create/move the annotations to a separate layer. When exporting the DXF, exclude the annotation layer from the export operation.

Re: Flat-Pattern remove bend annotations by default ?

Honored Contributor
Honored Contributor

We do two views, one with all the bend data, and one without for the water jet/laser cutter.  The one for cutting, we edit the view to not show the callouts, and anything else not needed.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Flat-Pattern remove bend annotations by default ?

Phenom
Phenom

If you use the flat pattern export function (to DXF or Trumpf GEO format) you don't have to deal with those bend call outs.

You will only see the geometry you choose; it will always have the correct face up; it will have the direction that you want (if defined in the flat pattern feature); it will always be scale 1:1.

 

So I would advise to use this NX Sheet Metal function. It's a huge time saver.

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend