Cancel
Showing results for 
Search instead for 
Did you mean: 

Flattening and Forming

Honored Contributor
Honored Contributor

We have been trying to flatten out a non-planer surface, using various techniques.  Flattening and Forming seems to be the best, compared to convert to sheetmetal, and Fabric Flat Pattern, but when we water jet the piece, and shape it into the area we are trying to fill, it comes up a bit short.  Looking at the length analysis in the tool, it doesn't appear there would be any issues, but I also get an "Output body has self intersections" warning.  Also, if I measure an edge of the face I am flattening, it's 25.211", and the equivelant flattened edge is 25.175".

 

Am I missing something?Flattening and Forming.JPG

-Dave
NX 11 | Teamcenter 11 | Windows 10
2 REPLIES

Re: Flattening and Forming

Phenom
Phenom

Where is the part?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Flattening and Forming

Honored Contributor
Honored Contributor

I had to do a little cleanup, before I could post it here.

-Dave
NX 11 | Teamcenter 11 | Windows 10